在3G网络刚刚诞生时,高清无线监控企业曾对3G寄予厚望,希望能为高清监控带来根本性变化,但事与愿违。据介绍,实际上目前的高清无线监控主要集中于车载监控以及复杂地形的远程监控和家居安防的防盗报警联网系统。4G的出现无疑给行业发展带来另一份惊喜,4G将会怎样融入安防技术,我们拭目以待。
一、2013年国内4G投资可能进一步超预期
从国家政策导向来看,国内很可能会有两家运营商运营TD-LTE制式的4G网络。国家对TD-LTE的重视将超越TDSCDMA,主要在于TD-LTE产业链发展远好于TDS,为了更好支持TD-LTE,国家对其要求已经从TDS时代的三分天下有其一,调整到三分天下有其一调整到有其二。而从国家对频谱分配上来看,分配190M的D频段赋予TD-LTE,190M频宽远远超出一家运营商需求,至少可以满足两家甚至多家运营商的需要。综上我们认为,从政策导向来看很可能至少会有两家运营商运营TD-LTE制式的4G网络。
我们认为,中电信可能会拿到另一张TD-LTE牌照。除中移动外的另外两家运营商中,只有电信的CDMA2000网络没有后续升级方向,联通的WCDMA网络升级到FDDLTE是较好选择;且中电信网络升级到TD-LTE还是FDDLTE要求相似,不存在升级到TD-LTE网络是否造成投资浪费的问题;另外,尽管其3G网络覆盖较为全面,但考虑到其网内高数据量用户如iPhone用户近期才规模启动,预计未来数据压力将推动其4G部署需求。我们认为,从电信网络的实际情况来看,其较有可能会拿到另外一张TD-LTE牌照。
如果我们以上的判断正确,中电信2013年将会启动试验网建设,提升投资预期。中移动已确定在2013年大规模推动建设,并在2012年已经实施了规模试验网的建设,若中电信获得另外一张牌照,国家也将会批准其提前启动试验网建设;而从电信本身来说,为避免在未来4G运营中对比中移动落后,本身也将有动力在2013年启动试验网建设。我们预计,若中电信在2013年启动试验网建设,其规模可能对比中移动在2012年多城市的试验网建设规模,考虑电信投资能力,其试验网投资规模有望在100-200亿之间,大幅提升投资预期。
二、4G推动高清无线监控新发展
3G网络应用的局限性可想而知,而对于中国移动新布局的4G网络企业同样有着新的期待。业内人士认为,3G网络在实现高清监控时具有其本身的局限性,但是4G网络却很好的解决了上述问题。据目前试点来看,4G网络的速度是3G网络的10倍,下载速度达100M,上传速度为20M,而一般的720P的高清监控需要的带宽基本每路在2M—4M之间,这就很好的满足高清监控的良好需求。
3G网络的稳定性实际上是很多消费者考虑的问题。由于网络基站的均衡性不一,造成了3G网络在传输上容易造成信号强弱不均,从而回导致掉帧、画面卡的现象。但是记者从中国移动公布的4G网络建设目标中注意到,2013年新建基站18万个,这就很好的解决了4G的网路信号问题。业内人士表示,未来的4G通信能满足第三代移动通信尚不能达到的在覆盖范围、通信质量、多媒体传输等需求。
流量的使用费用是很多人关心的话题,由于各个运营商制定的套餐不太相同,造成了运营服务费的居高不下,也使得无线高清监控推广举步维艰。据了解,4G网络采用逐步引入的方法,在原有3G的基础上对技术进行升级改造,成本自然会降低不少。相关人士表示,未来4G网络的费用会低于目前3G套餐费用。4G网络对无线高清监控的影响是显而易见的。如果4G网络能够在稳定性、流量费用等问题很好的解决,那对高清监控的影响将会是革命性的。
三、4G技术将普遍应用于安防
4G时代的即将到来,网络都将升级,以前基于二,三代网络传输的设备将渐渐失去市场。将来在4G浪潮的冲击下,安防行业的老旧产品的升级转型是必然的,优胜劣汰这是社会的选择。安防产品将随着通信技术的不断发展,而不断的升级改造,来满足的市场需求。
谁拥有的通信技术,谁就能掌控未来。4G技术正快速向安防企业走来,相信在不久的将来,4G技术必将成为通信技术的主流,而4G技术也将会在安防产品逐渐应用起
四、4G安防应用大势所趋
移动:布局4G网络
中国移动近日宣布将全面启动4G网络建设,相对于刚刚成熟的3G网络,4G在上传和下载速度都有较大的提升。中国移动杭州分公司技术部负责人接受媒体采访时表示,目前3G的下载速度在5M-10M,相比之下,新技术的网络要快10倍。这就意味着4G网络的速度可达到100M。神一般的4G网络能否为高清无线监控开辟新的蓝海,业内人士拭目以待。
下半年开始,中国移动全面启动4G网络建设。其中包括:2013年开始在国内100个城市进行TD-LTE我国4G技术标准设备采购,以及2013年建成TD-LTE基站规模超过20万个,即2013年新建基站18万个。据介绍,这一投资总额将达到约1800亿元。
据了解,到2012年底,中国移动将按计划完成建设TD-LTE基站2万个左右,这意味着2013年,中国移动将新建TD-LTE基站约18万个,如果按照每个100万元的建设成本计算,仅建设基站一项的投资,将达到1800亿元左右。更早时候,中国移动已透露,2012年到2013年,将投入2000亿元进行4G基站建设。
巨额投资布局4G网络市场,是中国移动避开其他运营商的3G网络建设的新举措。中国移动杭州分公司技术部相关负责人在接受媒体采访时表示:“使用TD-LTE通信网,意味着可以享受更加稳定和高速的无线移动网络,理论下载峰值可达到每秒百兆,下载一部电影可能仅需几秒钟时间。”而目前常用的3G网络下载速度在5M-10M,相比之下,新技术的网络要快10倍。
3G网络稳定性受到极大地限制,此外还有服务费的问题,在图像回放和观看时并没有想象中的优越。采用3G网络,如果有转发服务器支持,可以支持多路回放。但是如果没有转发服务器一般只能1-2路的观看。
深圳:4G应用推动新一代安防技术发展
深圳是全国7个TD-LTE试点城市之一,TD-LTE商用网将首先覆盖大运中心、开闭幕式场馆、媒体中心等大运会主要场馆及周边的滨海大道等主要道路。“4G”TD-LTE的特点是高速数据传输服务,是现有3G网络的十倍。有了TD-LTE,市民上网会比现在的有线宽带还快,可以通过手机等各种终端获得无线高清视频体验,无论是点播电视,还是在线视频会议,都会十分流畅清晰。
在今年的深圳大运会市民不仅可以用手机等多种终端观看大运赛事,相对于2008年的手机看奥运来说,这次在多种终端观看赛事的网速更快,播放更流畅。4G技术的应用使深圳大运会成为信息化程度的一届大运会。
TD-LTE是国家“十二五”支柱性产业“新一代信息技术”的关键组成部分。TD-LTE的发展,将促进移动宽带的发展,并与物联网、云计算等前沿技术相结合,形成新一代信息网络,带动互联网、软件、相关电子信息的迅猛发展。相信未来的几年时间内,4G技术将逐渐发展成熟,到时将会“蔓延”到安防行业,安防行业又将迎来一场新的技术变革。
南京:斥80亿建完整4G网,移动监控将迎变革
到2015年,南京移动将斥资80亿元,逐步建成满足城市需求的完整4G网络。从安防行业大环境来看,网络监控已是行业发展的大趋势。但是网络监控的实际市场占有率还是相当低,行业内人士认为,这是国内网络环境还不够成熟所导致的。同时,目前国内监控高清趋势愈发明显,许多知名监控厂商都已经开始推出更高清的700线摄像机,有些厂商甚至已经开始在行业率先推出千万像素摄像机。这些高清监控前端的广泛应用对后端来说,传输的压力将变的更重。4G网络的到来将给厂商们带来福音。
网络监控的分支移动监控领域,网络传输的压力更加突出。而4G网络的到来将其移动无线传输的优势应用于移动监控领域,同时正好为视频监控会议的发展带来了更好的网络环境。如果4G网络能够在国内全面普及,其“给力”的无线信息传输速度将极有可能带的移动监控产业的大跨步发展。4G网络技术将为安防行业注入新的活力,给安防行业带来新的变革,新的市场。