我国4G技术和国外几乎同步
据了解,目前国际上的4G通信标准有TD-LTE和FDD-LTE两种。FDD-LTE标准已于去年年初在欧美国家正式商用。截至2011年10月,全球有248家运营商已确定了部署LTE商用网络计划。业内专家表示,现在我国的4G技术已经比较成熟了,技术上没有问题。因为牌照发放等问题,我国4G的应用相对滞后一点,但在技术上和国外相比几乎同步。
据了解,目前,无论是从芯片到终端的产业链,还是频率规划和运营商建网的标准采用,全球的LTE产业布局仍在进行时。专家认为,未来3年我们将面临TDD-LTE发展的黄金时间窗口。
政府发力助推4G网络建设
我们知道,智慧城市建设被国家列入了十二五规划,相关的政策对智慧城市项目建设的投入资金与支持力度不断在加大。国家对4G网络建设项目的支持力度必将超越3G网络,因为4G技术所延伸出来的产业链给社会带来的经济效益远远超过3G所能达到的范围。4G时代的发展速度预计将比3G更为迅速,甚至远超出安防行业人士的预料。各地政府近几年大力推动智慧城市建设,许多地区的政府部门规划中,都把4G技术作为搭建一个融合了移动互联网和物联网的信息应用平台,让市民在购物、出行、学习、教育、保健等方面享受到更舒适、更便利的服务,同时也让政府城市管理更加精细化、智能化。
现在,政府部门已经谋划4G发牌机制和时间,设备商也在不断试验4G的产品和方案,中移动、中联通等运营商甚至启动4G技术试验与商业的准备工作等等。从目前来看,国家政策谋划是国内很可能首先由联通和移动两家运营商先获得运营TD-LTE制式的4G网络的资格。中移动已在2012年已经实施了规模试验网的建设,在2013年着手准备大规模推动建设。或许中国电信在不久也将能获得另外一张4G牌照。如果今后中国电信也启动试验网建设,其规模可能对比中移动在2012年多城市的试验网建设规模更大。而从国家对频谱分配上来看,已经分配190M的D频段给予TD-LTE,190M频宽远远超出仅一家运营商需求范围,至少可以满足两家甚至多家运营商的需要。
因此,4G技术的应用对安防产业来说是一个巨大的商机,安防系统的信息采集和数据存储都将迎来全新的时代。消费者意识的提升,也会使更多的企业关注民用安防这个蓝海。此外,政府资金的投入将支持4G技术趋于更加完善,网络系统更加稳定地运行,而这也为4G技术在安防行业的应用起到了“推波助澜”的效果。
4G技术将普遍应用于安防
4G时代的即将到来,网络都将升级,以前基于二,三代网络传输的设备将渐渐失去市场。将来在4G浪潮的冲击下,安防行业的老旧产品的升级转型是必然的,优胜劣汰这是社会的选择。安防产品将随着通信技术的不断发展,而不断的升级改造,来满足的市场需求。
谁拥有的通信技术,谁就能掌控未来。4G技术正快速向安防企业走来,相信在不久的将来,4G技术必将成为通信技术的主流,而4G技术也将会在安防产品逐渐应用起来,希望安防企业能够审时度势,抓住新的技术,发掘新的市场,寻找4G安防蓝海。
4G监控将弥补安防应用空白
无线网络的带宽与频率资源更为有限,带宽不够不能保证监控画面质量。以3G网络为例,在高速移动的过程中传输速率为144kbps,若想保证CIF画面需求传输速率至少保证512kbps。技术不成熟,网络带宽不足是无线移动监控的致命因素。然而,4G网络可实现100Mbps的速度下载。4CIF的画质只需要2Mbps的传输速率,对比可知,也许实现无线高清监控都不在是梦。
由于费用过高,无线网络监控得不到广泛推广。3G视频监控资费过高,一般用户无法承受;行业用户难于承担视频监控项目后期的持续网络资费支出。但有相关人士表示,4G资费有望有较大下调,让4G网络更“亲民”。4G网络传输价格下调必将更易接受。
目前的3G视频移动终端还不完全适用于3G视频监控,比如在前端存储上,普通硬盘体积过大,导致整机不利于安装;4G网络建设将更灵活,全球漫游,接口开放,能跟多种网络互联,终端多样化以及能从第二代平稳过渡等特点。
4G网络建设能够较好地弥补3G的不足,尽管4G也存在一定的技术短板,但是随着技术的发展我们有理由相信,在不久的将来4G网络会成为无线监控的后备军。
4G网络技术给安防市场带来新的变革
网络监控的分支移动监控领域,网络传输的压力更加突出。而4G网络的到来将其移动无线传输的优势应用于移动监控领域,同时正好为视频监控会议的发展带来了更好的网络环境。如果4G网络能够在国内全面普及,其“给力”的无线信息传输速度将极有可能带的移动监控产业的大跨步发展。4G网络技术将为安防行业注入新的活力,给安防行业带来新的变革,新的市场。
4G时代的即将到来,网络都将升级,以前基于二,三代网络传输的设备将渐渐失去市场。将来在4G浪潮的冲击下,安防行业的老旧产品的升级转型是必然的,优胜劣汰这是社会的选择。安防产品将随着通信技术的不断发展,而不断的升级改造,来满足的市场需求。
谁拥有的通信技术,谁就能掌控未来。4G技术正快速向安防企业走来,相信在不久的将来,4G技术必将成为通信技术的主流,而4G技术也将会在安防产品逐渐应用起来,希望安防企业能够审时度势,抓住新的技术,发掘新的市场,寻找4G安防蓝海。