处理中...

首页 > 资料大全 > 解决方案 >

降低LED驱动噪音的解决方案

降低LED驱动噪音的解决方案
来源:我爱方案网 时间:2013-01-07

【导读】LED驱动噪音是目前的一大难点,本文就如何降低LED驱动噪音提出了一些建设性意见,从根本上了解噪音发生的原因,如何抑制和降低噪音,本文给出了解决方案。

噪音来源

LED驱动的噪音来自哪里?

噪声来源来自一些磁性元件(如 变压器 ,电感器…)和多层陶瓷电容器(MLCC)。

为什么会产生噪音?

磁组件产生噪音主要有以下几个方面:

Percussion - The face of core pieces can scrape together when the magnetic flux is varied;
Collision of movable elements (bobbin, core , wire ..etc.);
Magnetostriction- The dimension of coil material is changed;
Coil self Motion-The ripple current pass through coil produces attractive and repulsive force that to move the wires.

多层陶瓷电容器也会产生噪音,原因在于:

Piezoelectric effect – Substrate vibrate with Voltage amplitude, and when the time amplitude cycle come to the bandwidth of auditory are, Harmony is recognized as a noise. Capacitor distortion transferred to the PCB acting as an amplifier。

降低噪音的方法

虽然目前我们没有方法来消除噪音,但是我们可以降低噪音水平。具体方案就是降低磁性元件的噪音水平:

Reducing peak flux of magnetic as low as possible;
Potting the PCBA;
Vacuum Varnish for magnetic parts. Method to reduce noise level for MLCCic parts;
Reduce capacitance value in a capacitor;
Add a soft material to absolved the mechanical vibration;
Replace the MLCC with a plastic film (Polypropyleneor, Polyester…etc);
Potting : Pot the PCBA.

热门推荐

更多 >
ESP32-S3 2022-03-16
RG200U 2022-03-16
USR-C322 2022-03-16

资料浏览排行榜

更多 >
商品名称 大小 浏览量
1 EPCS128SI16N 0.94MB 22192次
2 1N4001 0.19MB 18106次
3 DAC1220E 0.95MB 16429次
4 EP1C6Q240I7N 2.47MB 15974次
5 GRM32RR71H105... 0.10MB 14167次
6 DR127-3R3-R 0.72MB 11842次
7 DMG2305UX-7 0.40MB 9412次
8 DS1337U+ 0.28MB 9192次
9 DMP2008UFG-7 0.24MB 9189次
10 DX4R105JJCR18... 0.26MB 9104次