处理中...

首页 > 资料大全 > 解决方案 >

如何进行FPGA原型设计

如何进行FPGA原型设计
来源:EEFOCUS 时间:2015-07-07

自上世纪80年代末,芯片制造商开始使用FPGA器件来搭建ASIC设计系统原型,FPGA原型设计已经走过了漫长的道路。一个FPGA工作原型可以让硬件设计开发和测试他们的系统,也可以让软件开发者提前获得一个全功能的硬件平台。

 

上世纪80年代末,当FPGA出现在半导体领域的时候,它发生了很多变化。芯片开发商需要处理百万门的大规模ASIC / SoC设计。这个时候,分区设计,调试和扩展性等要求使得以FPGA为基础的原型技术成为一个更可行的设计工具。

 

A prototype is used to develop both hardware and software iteratively

 

S2C Inc.'s e-book titled "Getting the Most Out of FPGA Prototyping" can serve as a handbook on how this design methodology works. Moreover, it debunks the myths surrounding the issues regarding how FPGA prototyping works and what value it brings to ASIC/SoC designers. S2C has cobbled the e-book on FPGA prototyping systems using a series of articles published in EE Times.

 

The series of articles can help chip designers navigate the world of FPGA prototyping technology—everything from overcoming FPGA prototyping hurdles to expanding the use of FPGA prototype design flow to even the larger designs.

 

Furthermore, the e-book from S2C looks into the specifics of how FPGA-based prototyping can accelerate design and verification process. And by doing that it offers an insight into how a complete prototyping platform can be helpful at any design stage and for any design size.

 

FPGA Prototyping: Challenges and Solutions

The book kicks off with an outline of five key challenges to FPGA prototyping and provides a detailed treatment of issues such as partitioning, debug and reusability. Next, it delves into ways for addressing these challenges and details the criteria for selecting FPGA-based prototyping systems.

 

The e-book also clears the air about this myth that FPGA prototyping is only suited to small designs; it forcefully makes the case for the use of FPGA prototyping in large SoC designs. Here, the book refers to the recent advancements in partitioning, debug, and scalability that have made FPGA-based prototyping a far more suitable solution for the large ASIC/SoC designs.

 

The book also shows how extending the functionality of FPGA prototyping through the use of a transactor interface can open up tremendous possibilities to designers. Next up, Getting the Most Out of FPGA Prototyping resorts to transactor as a use case of an interface between a software program and AXI-compliant hardware.

 


Transactors make early software development a reality

 

Finally, about the SoC designs, which are growing both in size and complexity, it's worth noting that software development and hardware verification are the two leading factors in SoC design cost. Here, at this SoC premise, the book shows how today's off-the-shelf FPGA prototyping systems can offer value in every stage of the SoC design flow. And it claims that FPGA-based prototyping technology is ready to cater to the next-generation SoC designs through extensible and scalable systems that offer a variety of both hardware and software interfaces.

 

热门推荐

更多 >
ESP32-S3 2022-03-16
RG200U 2022-03-16
USR-C322 2022-03-16

资料浏览排行榜

更多 >
商品名称 大小 浏览量
1 EPCS128SI16N 0.94MB 22196次
2 1N4001 0.19MB 18110次
3 DAC1220E 0.95MB 16434次
4 EP1C6Q240I7N 2.47MB 15978次
5 GRM32RR71H105... 0.10MB 14169次
6 DR127-3R3-R 0.72MB 11845次
7 DMG2305UX-7 0.40MB 9415次
8 DS1337U+ 0.28MB 9196次
9 DMP2008UFG-7 0.24MB 9193次
10 DX4R105JJCR18... 0.26MB 9107次