来源:cnbeta
时间:2013-02-18
近日,松下公司成功开发微型彩色分离器,在光线不足的情况下创造出明亮的影像效果。这不需要滤色器的参与,与传统滤色器相比可以提高颜色灵敏度高达2倍。这可能对移动设备上的相机和类似设备产生积极的影响。
传统传感器所使用的彩色滤光片为50%至70%之间的环境光,随着的发超灵敏的彩色微型分光传感器的产生,这个问题将是不存在的,而成像的图片将显得格外生动,丰富多彩。根据官方的报道,这种方法与常规传感器相比,只需要一半的环境光线。
彩色微型分光不局限于指定类别传感器,并且可以使用CMOS和CCD传感器。目前该技术拥有16个国际专利和21项日本专利。