来源:C114中国通信网
时间:2013-01-17
全球移动供应商协会(GSA)表示,截至目前,全球已有66个国家的145家运营商推出了商用LTE服务。据GSA更进一步的报告显示,2012年新增了104家运营商承诺投资LTE网络部署,使承诺部署的运营商总数增至104个国家的330家。
报告称,1800 MHz是LTE部署的主流频段,并且预计这一趋势将会持续。在全球39个国家,商用LTE网络的运营商中,有40%使用1800 MHz作为单一的频段系统,或者作为其多频段网络部署中的一部分。其次常用的LTE网络部署频段为2.6 GHz (band 7)。
相比12个月前,在2012年,有97张网络在超过37个国家推出。截止2011年底,全球共有47张商用LTE网络。
GSA预计,到2013年年底,将有234张商用LTE网络在83个国家推出。