中移动4G全国性商用,中电信4G将在2月上旬放号。内部人士透露,中联通4G放号迟在今年3月正式在国内重点城市启动,今年上半年推出4G套餐,相关资费正在研究中。 中联通副总裁张范在北京两会上表示,中联通很快将推出4G套餐。 “4G本身速度更快,在单位成本各方面比3G更低,所以资费上也会更实惠。” 2013年10月,中联通开始向各家设备厂商发出了4G网络设备招标计划,首次集采计划采购4G基站5.2万个。 中联通副总裁姜正新在接受笔者采访时表示,中联通4G实验网已在全国重点城市启动,FDD/TDD制式网络都有;中联通总经理陆益民表示,中联通的4G网络建设思路是渐进式的推进过程,未来将构建“2G 3G 4G”无缝覆盖、用户体验好的网络。 有报道称,FDD-LTE(4G)牌照将在2月14日前夕发放。不过,中联通内部人士给予否认称,“到5.17电信日发放FDD牌照就不错了。” 不过,也有分析认为,FDD-LTE牌照没有发放之前,中电信、中联通4G网络较为“被动”,推进速度也不会太快。一方面要从3G网络向4G网络演进(主要是FDD-LTE)。另一方面,高层仍然对TD-LTE表现出非常谨慎的态度。 因此,“两会”之前发放FDD-LTE牌照符合市场实际。由于TD-LTE牌照发放,没有任何征兆。工信部将虚拟运营商牌照放在1月29日发。因此,2月份后任意一天发放FDD-LTE牌照都变得有可能。