与3G牌照发放整整讨论了10年不同,4G牌照发放在2009年3G规模建设4年后就进行了发放,也颇匹配于行业的加速度。那么,4G到底会在哪些方面、在何种程度上改变中国呢?其实,4G的影响可能没有那么大,有四个难以改变。4G不会改变的四件事当年2G牌照发放的时候,伴随着老的邮电部企业化,中国移动、中国联通先后成立,其中,拿到GSM牌照的中国移动获得了火速的发展,迄今用户数量已经稳居全球,总营收亦位居全球前五之列,仅次于AT&T、NTT、NTT DOCOMO等少数几家厂商,而净利润已经多年高居全球榜首。但是,选择了CDMA这一美版2G的中国联通、同时也拥有GSM牌照,则长期处于相对的弱势,其CDMA网络仅仅成为中国加入WTO与美国政府的一次政治交换筹码。这个过程中,三大门户、腾讯等企业都曾经借助中国移动梦网的SP业务度过了互联网的冬天;中兴、华为首次进入移动通信市场,成为国际化跳板。而3G发放的时候,伴随着运营商的重组,中国电信从联通手中接手CDMA,实力强的中移动获得了TD牌照,实力弱的联通拿到制式好的WCDMA。客观讲,这次制度安排依然有政策考量,一则为了支持国产的TD标准;一则让中国电信获得移动牌照,让三家运营商之间实力更加均衡,竞争更加激烈,这个目的基本达到了。一个额外的效果就是中国的移动互联网实现了大爆发,但是,同时,也让运营商和互联网厂商从双赢为主走向了竞合型关系;而其间,中国电信设备商中,华为从全球第三名成为全球,中兴从第八跻身第五,展讯、锐迪科、创毅等大陆芯片厂商也跟随冒头了。现在,4G牌照发放的时候,相关的政策因素已经大幅减少,主要就是让三家运营商都率先拿到TD-LTE牌照,如果不出意外,后续也都会拿到FDD LTE牌照。而4G的两种制式之间的差距已经变得非常小了,这时候,中移动当然会非常主动进行4G建设,但是,其建成后的优势并不会那么大,毕竟联通的WCDMA的升级版本DC-HSDPA等,其下载速度也能高达84Mbps甚至更高,和LTE差距并不算大。所以,4G不会改变很多事:,高通、联发科的芯片会进一步多模融合,不同制式手机之间的差距会缩小,这让高通获得了一定的技术优势,但是,由于毕竟先发TD牌照,展讯、创毅等也未因此有新的弱势,主要靠自身努力;第二,运营商之间的技术差距变小,终端差异也在变小,比如,中国移动已经和苹果签约,但是,这也不会让联通、电信形成明显弱势,因为,新增客户已经日渐稀少,换机动力也在减缓,且移动4G建设也需要较长的时间才能全面覆盖;第三,这不会更大程度上提升中兴、华为等厂商的优势,毕竟二者在中国已经占据半数市场,在美国、日本、韩国、澳洲等美国的“友邦”受制于政治因素难以大规模进入,只能取决于在亚非拉和部分欧洲市场的拓展力;第四,这也不会大幅改变互联网厂商的格局,3G时代的网络格局改变在于智能机+数据通信的普及化,2G和3G之间的用户体验瓶颈比较大,但是在WIFI大行其道、家庭宽带日益普及的时候,4G的用户体验提升不再是大幅的改进,而是中小幅的提升了。4G将可能会改变什么?我们提到了四大难以改变,是因为那些方面,网速不再是主导的因素——就像我们家用的宽带,56K的猫到2M的ADSL之间是存在巨大的飞跃,因为那里有明显的瓶颈;但是,等从8M到所谓100M宽带的时候,这个影响就没有那么大了——正如,日韩的100M光纤非常普及,但是,这不意味着它的应用就一定比美国丰富多少。那么,这是否意味着4G对产业和消费者的影响可以忽略不计了呢?当然不是。4G潜在的影响力主要源自三大方面:个,将会被深度改变的用户消费习惯,并由此影响到互联网的内部结构。其实,这一点,在3G时代的晚期已经出现了很大的变化,比如,Youtube也好、优酷也好,这些重量级的产品,在移动端的流量都达到了40%-50%这样的比重;新闻客户端、公众账号的阅读更是超过了PC端;微博的手机侧流量超过70%;移动侧游戏迅速超过网页游戏,并保持飞速发展……换句话来说,用户当有更方便获取信息的渠道、且用户体验超过临界点之后,没有必要长期继续固守PC。无疑,4G会大大加速移动互联网的进程,并让很多3G设备可以转移到郊区、更小的城市,也进一步促进这种普及从核心和发达地区向周边扩散。第二个,以视频为核心的各类应用可能打开想象空间。人们想到视频,往往时间想到普通用户的视频电话,其实,这个产品的价值并不大,无论是国内还是海外,这种应用都没有真正广泛流行过,这是因为,视频通话不是强需求。但是,其它类的视频应用则不然,可能有很好的发展,比如,公司级的视频会议,以前的时候,都需要专门的会议室、网真类的视频设备等等,成本巨大,未来完全可以借助个人的终端和云端服务就能低成本解决;而很多家庭幼儿的监护,也完全可能通过手机和APP实现……这些现象空间嫁接于软件和APP,而非P2P视频通话这种单一的应用。第三个,很重要的一点,是物联网等衍生应用的发展。严格意义上说,物联网和4G没有必然的联系,物物通信本身需要借助的是新的技术,但是,也存在一种可能性在于,原来物联网应用较高的成本可能通过软件和APP方式来解决,从而变相推动物联网的发展。比较典型的是车联网,在移动状态下的数据交换,无需借助GPS等方式,而通过移动网络。