处理中...

  • BCP56T1G

  • 牌: ON SEMICONDUCTOR
  • 本: 1.4
  • 述: These NPN Silicon Epitaxial transistors are designed for use in audio amplifier applications. The device is housed in the SOT−223 package, which is designed for medium power surface mount applications.
  • 文件格式: PDF
  • 文件大小: 0.07MB
  • 数: 6
  • 查价格
PDF原版资料

资料浏览排行榜

商品名称 大小 浏览量
1 EPCS128SI16N 0.94MB 22234次
2 1N4001 0.19MB 18146次
3 DAC1220E 0.95MB 16469次
4 EP1C6Q240I7N 2.47MB 16017次
5 GRM32RR71H105KA01L 0.10MB 14200次
6 DR127-3R3-R 0.72MB 11881次
7 DMG2305UX-7 0.40MB 9451次
8 DS1337U+ 0.28MB 9231次
9 DMP2008UFG-7 0.24MB 9228次
10 DX4R105JJCR1800 0.26MB 9143次